6/8/2018 7:56 AM | |
Joined: 3/27/2013 Last visit: 11/22/2024 Posts: 5 Rating:
|
Same problem. Ask for help. After loading the configuration into the PLC, the controller does not start. what am I doing wrong? I do not understand what parameters are incorrect. Ping with 343-1 a good. OB86 is present in the project 343-1ex30-0xe0 place in rack2 modul 7 . ------------------------------------------------------------------------------------------ AttachmentDiagnose.txt (107 Downloads) |
Last edited by: nncbot at: 6/8/2018 7:58:05 AMLast edited by: nncbot at: 6/8/2018 8:05:04 AMLast edited by: The Helping Hand at: 6/11/2018 9:55:55 AMNew subject after splitting |
|
6/8/2018 8:10 AM | |
Joined: 3/27/2013 Last visit: 11/22/2024 Posts: 5 Rating:
|
Screenshot hwconfig |
6/10/2018 9:37 AM | |
Joined: 3/27/2013 Last visit: 11/22/2024 Posts: 5 Rating:
|
Compiling and loading the whole project did not help. The problem is still relevant. Does anyone have any suggestions?
AttachmentDiagnose.txt (99 Downloads) |
Follow us on