Industry Online Support
Technical Forum
9/30/2010 10:18 PM | |
Joined: 7/28/2010 Last visit: 3/18/2024 Posts: 184 Rating: (11) |
CH, KNKT =B#(0,3) 0: means channel 0 from this analog input card 3: means absolute value representation (4-20mA) In S7 converted code, you have set the card address at 256 which ischannel 0 of the card. KNKD value should be either 22, 23, 24, or 25 In your case it should be 25. It is either W#16#25, or hex value of 25 which isw#16#19. About second question, i don't know what FC6 stands for or supposed to do? Regards, Behnam www.sigmaprocess.ca |
Follow us on