2/25/2025 8:09 AM | |
Joined: 5/6/2022 Last visit: 4/16/2025 Posts: 585 Rating:
|
Hi DaFo_ALO, As indicated in the following link, recipes in Unified have a different concept: In this case, I think that the best way to migrate those recipes from Comfort Panel to Unified Panel is performing the following steps: 1. Export the recipes from Comfort device as csv file. 2. Adjust your recipes accordingly. 3. Export the new created parameter set type from Unified device as tsv file. 4. Add all recipes at once to the tsv file. 5. Import new created parameter sets through Runtime to the Unified Panel using the modified tsv file. This may be an option to try to migrate recipes. |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on