Industry Online Support
Technical Forum
3/20/2013 2:03 AM | |
Posts: 7 Rating: (0) |
Hello. I have a problem with the conversion of S5 to S7. LIR The program includes instruction and TNB, which are not automatically converted. The program was written for the S5-95U and I want to convert it to the S7-314. Function blocks FB 110 and FB 111 (FC 30 FC 31 and after conversion) are called by the open DB 2. What will be the contents of ACCU 1 and ACCU 2 after executing LIR 0 - such as FB 16 (FC 14) Segment 2? On which area of data is executed statement TNB? How to replace LIR instructions and TNB in S7? I enclose portions of files after conversion. Thank you in advance for help. AttachmentListingi.zip (428 Downloads) |
Last edited by: O_Moderator at: 3/20/2013 9:31 AMnew subject after splitting from /tf/WW/en/Posts/88989#top |
|
Follow us on