3/22/2021 9:25 AM | |
Posts: 3 Rating:
|
Hi. There is a VB Script that I tested with PC Simulator. I'm going to put this in the TP900 and test it VB Script must be changed from PC Base to WINCE base. Give me advice in this regard. The text file of the attached file is a script that I need to convert. Any help with the conversion in this regard would be appreciated. AttachmentWRITE CSV_VBSCRIPT PC Base.txt (101 Downloads) |
3/22/2021 4:48 PM | |
Joined: 7/5/2013 Last visit: 4/22/2025 Posts: 3148 Rating:
|
Hello kjkim, check Differences between the VB script functions of Windows and WinCE. There you find a description about the functions which can be used in WinCE. For checking whether file exists you can also find ways in that description or search for it in the forum. Regards, Frink |
Pi is exactly three! |
|
This contribution was helpful to
1 thankful Users |
3/26/2021 12:36 PM | |
Joined: 8/3/2009 Last visit: 4/17/2025 Posts: 15311 Rating:
|
Hello kjkim46 Here are the two different examples: PC Based: hhttps://support.industry.siemens.com/cs/ww/en/view/59604194 Panel based: https://support.industry.siemens.com/cs/ww/en/view/59604194 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on