10/12/2018 9:17 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Set P0971 = 1 which saves data from RAM to EEPROM. To save from starter please refer attached sheet. |
10/12/2018 9:29 AM | |
Posts: 80 Rating: (1) |
I tried it, showed it on the "busy" display and showed the error F0051, as if it was a mistake on the EPROM. And the new card where EPROM is located |
10/12/2018 10:30 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Have you replaced card? If yes have you checked compatibility of the new one? |
10/12/2018 4:23 PM | |
Posts: 80 Rating: (1) |
a new card was replaced |
10/15/2018 9:14 AM | |
Posts: 80 Rating: (1) |
I've replaced the card (an image attached), the firmware is the same on both cards 2.11. The same number is MC1790L802V01 |
10/18/2018 12:54 PM | |
Posts: 80 Rating: (1) |
write on an old and new card |