10/4/2009 12:24 PM | |
Posts: 2348 Rating: (264) |
Via external card reader to MMC with same size (Siemens only). |
10/4/2009 6:22 PM | |
Posts: 50 Rating: (1) |
thanks for the reply but i am very new to the siemens can u explain what software and hardware will be required for the same thanks in advance |
10/4/2009 8:43 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hi, You need a prommer or a programming device that can write to the Siemens Memory Cards. This is not possible with all prommers and PC-PCMCIA interfaces. Look at follow order number description Regards |
7/13/2010 7:41 PM | |
Posts: 50 Rating: (1) |
You need a prommer or a programming device that can write to the Siemens Memory Cards. This is not possible with all prommers and PC-PCMCIA interfaces. Look at follow order number description Dear umencho, I spoke to our local siemens service engineer and showed him the manual suggested. we were not able to conclude that the prommer can be used to copy protected mmc. can you suggest any other document which shows the procedure to do the same. Thanks manish |
This contribution was helpful to1 thankful Users |
9/11/2015 1:58 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by Dany Min is split to a separate thread with the subject SIEMENS USB Prommer for S7-300 MMC. Best regards |
Follow us on