Industry Online Support
Technical Forum
10/16/2008 11:15 AM | |
Posts: 1776 Rating:
|
Hi, to 1. see the links http://support.automation.siemens.com/WW/view/en/2566777 http://support.automation.siemens.com/WW/view/en/13681075 to 2. Search in the Manuals for COROS https://support.automation.siemens.com/WW/llisapi.dll?aktprim=100&lang=en&referer=%2fWW%2f&func=cslib.cssearch&siteid=csius&extranet=standard&viewreg=WW&objaction=cssearch&content=skm%2Fmain%2Easp Coros Software is not more available to 3. need more details RT is Runtime software RC is Engineering software RT128 is for 128 tags. This needed for Clients |
10/17/2008 2:20 PM | |
Joined: 10/17/2006 Last visit: 1/28/2024 Posts: 97 Rating:
|
Hello, I think the best way to convert from LS-B to WinCC is to rebuild the project by hand (and brain). This is the only way to use the benefits of WinCC. I know there is a special department in Nuremberg, which does only conversion from LS-B to WinCC and they have a conversion tool. But it is not perfect, you have to correct all pictures and, as I see, your LS-B project is not really big so I think the easiest (and cheapest)way is to convert by reading LS-B and typing WinCC. your questions: 1. yes, sufficient (if you use WinCC V7 RT2048 will be sufficient) 2. because WinCC Server handles the data exchange with SIMATIC and the WinCC Client gets all Information from WinCC Server, so WinCC Client needs no external tags. 3. yes, you need user archive. LS-B Index archive are similiar to WinCC user archive. best regards pinky |
Last edited by: pinky at: 10/17/2008 2:21 PM |
|
10/17/2008 6:51 PM | |
Posts: 6 Rating:
|
Dear pinky, Thanks for ur support. i ve some more confusions. can u solve them out? 1.Could you please tell me which migration tool would be required? 2. Why TCP/IP cable must be used for communication with master and slave ? 3. If i use panel PC 677B which acessories are required and would it be sufficient? 4. Could u tell me MLFB of all above listed softwares and hardware? i shall be thankful in advance. Best Regards, Qasim |
10/20/2008 8:39 AM | |
Posts: 1776 Rating:
|
Hi, all your questions semms fine for a Siemens sales person. Please contact your Siemens sales person. Contact address you can find with the link https://www.automation.siemens.com/partner/guiGeoSearch.asp?regid=def&lang=en&reduce=prodid517341&comptcid=v |
Follow us on