3/9/2018 2:28 AM | |
Joined: 9/27/2006 Last visit: 3/18/2025 Posts: 12344 Rating:
|
Hello JoDooMan; Have a look at this site, entitled "How Far and How Fast Can You Go with RS-485?": https://www.maximintegrated.com/en/app-notes/index.mvp/id/3884 Profibus-DP ios built upon a RS-485 physical layer, so it is to be expected that the limitatioons of RS-485 affect it also. The main factors limiting data rate on RS-485 (therefore Profibus-DP) are listed in the attachment below. Among other factors, the impedance of the line is particularly important. The line capacitance increases with frequency (or speed), and shortens the length the signal can travel with recoverable attenuation: the faster the bus speed, the shorter the length of the segment. Conversively, the lower the bus speed, the more "forgiving" the network becomes, the easier it is for the signal to cross the same distance, as you have observed yourself. Hope this helps, |
This contribution was helpful to
2 thankful Users |
Follow us on