9/21/2010 11:10 AM | |
Joined: 4/20/2007 Last visit: 3/4/2025 Posts: 728 Rating:
|
Well, here I am again... I got a list from my costumer. I have to fill in function code, register adress + +. The other side of the modbus line is also Siemens, but I think its Desigo, and he knows nothing about S7 300... And I'm stuck, I really don't see any logic in this. See attachment. I filled a datablock with the data I want to send, the other one is ready for receiving. Why do I need to set memory bits, outputs, timers and counters? Could I just use the FC03,06,16 tab, and send my bits as an word? Or doesnt that make sense? Could someone please help me with this? I feel kinda stupid here... Ton Splitted from CPU 313C + CP 341 (modbus slave). Attachmentmodbus, slave.pdf (179 Downloads) |
Last edited by: O_Moderator at: 9/21/2010 2:16 PMnew subject after splitting |
|
Follow us on