7/11/2017 6:17 PM | |
Joined: 9/5/2010 Last visit: 9/11/2022 Posts: 30 Rating:
|
Hi to all, I am in the same situation right now, and mentioned in the above posts, I need to install the Siwarex U setup for Step7 file. My current Siwarex U software if of order no.: 7MH4950-1AK01, and the weighing modules present in the HW is only 7MH4950-2AA01 and 7MH4950-1AA01. I need to have the old weighing module, 7MH 4601-1BA01, since the machine program is having the old module installed. To link the old weighing module to my HW, Sewarixi mentioned that a software configuration package be installed, 7MH4683-3AA63. This is where my problem is, my software installed is for siwarex U - 4950 series, and I could not find a configuration software for siwarex U - 4601 series. Is there anybody here, who have already found a link, where to download the Siwarex U setup for step 7 file? Is it still available for purchase? Thanks for the help. Cheers. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/12/2017 12:30:31 PMNew subject after splitting |
|
7/12/2017 4:58 PM | |
Posts: 206 Rating:
|
Hi Abigail, if you want to integrate the old Siwarex U 7MH4601* into your HW-Configuration you have to install the HSP for it. The HSP you find here: https://support.industry.siemens.com/cs/de/en/view/48549017 Be aware, if you have installed the "SETUP-FOR-STEP7" from the old configuration package 7MH4683*, you have to uninstall it before installing the HSP. The access to the Siwarex U you can't do with the FB that is provided for the new Siwarex U 7MH4950*, you have to do it in the "old way" as described in the manual https://support.industry.siemens.com/cs/de/en/view/7787659 chapter 5. Regards ABenno |
This contribution was helpful to
3 thankful Users |
9/11/2017 1:53 PM | |
Posts: 87 Rating:
|
Thank you very much! This notes very helpful for me.... |
Follow us on