2/26/2009 2:30 PM | |
Joined: 5/8/2006 Last visit: 1/29/2021 Posts: 1085 Rating:
|
Hi |
2/27/2009 8:47 AM | |
Joined: 5/8/2006 Last visit: 1/29/2021 Posts: 1085 Rating:
|
Hi You find this information in the chapter 2.2 of the following manuel: http://support.automation.siemens.com/WW/view/en/1137637/0/en Bye |
3/2/2009 10:55 AM | |
Joined: 10/19/2005 Last visit: 11/30/2020 Posts: 1611 Rating:
|
Hi, i found this FAQ -> http://support.automation.siemens.com/WW/view/en/19687561 Maybe this could be helpful for you. I heard, that with the new SP1 for WinCC flexible 2008 there should bea new function. Ifa system message comes, you can project a "incoming" event -> for sample "call a script whichshould "change the conection" .... The SP1 should comes in the next two or three weeks. ( i hopeit). Maybe you can wait for this time. regards, |
3/3/2009 2:18 PM | |
Posts: 43 Rating:
|
hiii alll is there any one here could send me asample programe for redundant software and connecting the two stations to the hmi runtime thanks for ru effort |
Follow us on