1/19/2009 7:42 AM | |
Joined: 1/5/2009 Last visit: 9/23/2022 Posts: 29 Rating:
|
Hello Hulzhex, Yes, the first part is complete The PLC sending data to the server (I checked it with the wireshark), the server received data, but still waiting... the communication is only on the TCP protocol. Problem is maybe in the flags in the flags in IP protocol http://www.networksorcery.com/enp/protocol/ip.htm#Flags. If I tried send same data from other computer 1), the flags was 0x40, but data from the PLC 2)have flags 0x00. And the second thing is the "Timeto Live" value. From the PC is 128 and form the PLC is only 30. Have you got any idea? Thank you Dra_Be 1) In this issue the server send me corectly reply 2) In this issue the server send me empty message and waiting for other data |
Follow us on