7/28/2006 6:11 AM | |
Joined: 1/3/2006 Last visit: 2/19/2024 Posts: 726 Rating:
|
hi there,
As per the manual of the FM350-1 counter module (pg 51) "UDT was copied to block library called FMx50LIB when the FCs were installed.You must not modify UDT2. Copy UDT2 together with the FCs into your project" After installing the required software, whichcame with this module, I can view FCs (FC 0 ,1,2 & 3) in my library FMx50LIBbutnoUDT2. Where to locate the UDT2? Do I need to create it? But then manual says not to manipulete the orignal UDT2 !! Confused,please help. Regards, Manmeet Attachmentu3.zip (288 Downloads) |
7/28/2006 8:55 AM | |
Joined: 4/24/2006 Last visit: 7/12/2024 Posts: 8711 Rating:
|
Hello manmeet, It's not UDT2 but they mean UDT1 ![]() See also the getting started pag 3.: http://support.automation.siemens.com/WW/view/en/2746047 Hope this will help you, Best regards, Wizard |
2/5/2007 3:32 PM | |
Posts: 9 Rating:
|
[:xxx:] Nice to see this topic. Imade the same error. (Using only the manual as a last resort) Regards Ove BP |
3/23/2008 3:17 PM | |
Posts: 1 Rating:
|
Hello, Could anyone kindly confirm that it is UDT1 or UDT2? Thank you so much. |
This contribution was helpful to
1 thankful Users |
Follow us on