7/21/2021 9:51 PM | |
Joined: 12/18/2014 Last visit: 5/21/2022 Posts: 26837 Rating:
|
Yes, it's possible by using Parameter-VM-Mapping. It's a DInt value, a VD in mapping table. |
7/21/2021 9:59 PM | |
Joined: 4/20/2021 Last visit: 7/22/2021 Posts: 9 Rating:
|
Would you have time to send me a small example Logo ladder and LWE project? |
7/21/2021 10:04 PM | |
Joined: 4/20/2021 Last visit: 7/22/2021 Posts: 9 Rating:
|
Good night! Thanks |
7/22/2021 5:51 AM | |
Joined: 12/18/2014 Last visit: 5/21/2022 Posts: 26837 Rating:
|
In attachment the example.
AttachmentJPC Consulting.zip (49 Downloads) |
7/22/2021 1:14 PM | |
Joined: 12/18/2014 Last visit: 5/21/2022 Posts: 26837 Rating:
|
No, the addresses are freely selectable. You just have to be careful not to duplicate or overlap. Example: You have the bit signals V0.0 - V0.3. Then you are not allowed to use the VB0, neither the VW0 nor the VD0.
AttachmentLOGO! Bit, Byte, Word and DWord.pdf (49 Downloads) |
Follow us on