7/8/2013 5:44 PM | |
Posts: 691 Rating:
|
Dear All I am facing a problem at a site where I am unable to load XDB File for a PC Station because the PC is not detecting CP 1613 Network Card installed in it. The Engineering Station was communicating with the connected PLC with the Named Connection configured. Few days ago it stopped communicating with the CP 1613 Network Card installed on it but I was able to communicate with the Onboard LAN Network Card. I formatted the Enginnering Station and re-installed all the softwares again, but NDIS Driver was missing for the CP1613 Network Card and I was unable to communicate with the PLC and other Stations over Ethernet through CP1613. I got NDIS Driver for the CP1613 in a Simatic Net CD and I installed it. After Installing I got the CP 1613 LAN connection and I was able to communicate with the PC Stations over Ethernet, but it is not showing anything in the Configuration Console. Hope you understand my problem and clear it. I have attached the snapshots. AttachmentCP 1613.zip (121 Downloads) |
Follow us on