9/17/2014 3:14 PM | |
Posts: 11 Rating:
|
Hello! I'm having an issue with an CP 341-RS232C module which is connected to a small terminal box which sends out a ASCII code. To my knowledge i have all the correct installations (Siemens configuration package and FB's provided from example project :zXX21_01_PtP_Com_CP34x --> CP341 Protocol 3964) and followed all the guidelines (CP 341 -First steps in Commissioning, CP 341 Point-to-Point Communication, Installation and Parameter Assignment) None the less I do not see anything coming in at "DB41.DBW18" I do get an error counter and status in the provided VAR table (W#16#1E0F) and a status code in the instance DB22 (DW#16C0809300) None of these errors seem to be referenced or documented any ware. Does anyone have an idea? thx Danny p.s. I have attachements corresponding to the above
AttachmentSiemens.zip (105 Downloads) |
Follow us on