9/5/2017 4:32 PM | |
Posts: 3 Rating:
|
Dear PLC-gurus, I'm having a problem trying to configure communication between a CP342-5(mine) and a 400 CPU (customer side). I'm used working with Profibus DP but last minute the customer requested I'd use FDL. I changed the communication to an FDL link and matched all the parameters given by the customer such as PB adress and LSAP of both master and slave. I changed the DP_SEND and DP_RECV to the AG-versions Now my CP342-5 seems to be dropping out of the logical token ring and gets entered again cyclically and there is no data being sent offcourse (at one moment the customer did receive my data but it almost instantly stopped so I'm guessing the configuration is correct for the biggest part). The error code on my AG_SEND block is 8135, which seems to support the 'dropping out' I've attached some pictures with more info. Curious about what you guys think. Kind regards, RN AttachmentCP 342-5.zip (70 Downloads) |
9/5/2017 10:54 PM | |
Posts: 3 Rating:
|
Hi Daniel! I also noticed that but wasn't sure it would give any problems because I'm not using DP anymore? i wasn't really sure what it meant.. Best regards, RN |
Follow us on