2/27/2018 8:44 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating:
|
New question published by AutoGen_8562133 is split to a separate thread with the subject Is it possible to communicate between a redundant cpu(412-5h) and a single station (cpu 315 with cp 342-5) without Y-link?. Best regards |
3/1/2018 9:12 AM | |
Posts: 15 Rating:
|
hello, i send the CPU diagnostic buffer, these addreses are configured in the CP342 configuration thank you |
3/1/2018 11:37 AM | |
Posts: 15 Rating:
|
HI, the situation is that I´m working like Slave and I have communication with the master (in this case S7-400 ). If i lose the power supply of the cp342 (the CPU315 doesn´t lose power, only CP) and restart it, the CP342 cannot RUN, and is in STOP. the only way to RUN again is downloading the HW , nothing with the STOP/RUN swith, restart power again... thank you AttachmentDiagnose CPU315.txt (173 Downloads) |
3/1/2018 11:37 AM | |
Posts: 15 Rating:
|
the HW configuration
AttachmentCP342_HW.docx (163 Downloads) |
Follow us on