9/6/2016 1:06 PM | |
Joined: 11/5/2013 Last visit: 12/3/2024 Posts: 37 Rating:
|
Hello I'am facing up a probñem reñated with HW configuration of a CP 343-1 lean The configuration is very simple ,I want to add the Cp343 for comunícate a PLC with a SIEMENS panel by ethernet I've checked many times the HW configuration and I'am not able to get the PLC in run ( There is no program in the PLC only OB1 and empty) If I go to Accesible nodes ,as you can see in the attached Word ,the CP doesn't appears, so I understand HW configuration has not been transfered completly to PLC Please help, and theank you in advance Attachmentcp343.docx (396 Downloads) |
9/7/2016 10:19 AM | |
Joined: 11/5/2013 Last visit: 12/3/2024 Posts: 37 Rating:
|
Hello Thank you for your answer Here attached you can see the online Ethernet diagnostics of the module Hope this helps Attachmentcp343-II.docx (377 Downloads) |
9/7/2016 10:31 AM | |
Joined: 11/5/2013 Last visit: 12/3/2024 Posts: 37 Rating:
|
IF I try to connect by MPI to the CP is not posible Thank you in advance ! Attachmentcp343_III.docx (260 Downloads) |
Last edited by: luismarcelo at: 9/7/2016 10:32:08 AMLast edited by: luismarcelo at: 9/7/2016 10:46:00 AM |
|
9/7/2016 4:54 PM | |
Joined: 3/21/2006 Last visit: 3/19/2025 Posts: 10239 Rating:
|
Hello, Try it reload the last firmware https://support.industry.siemens.com/cs/gb/en/view/59038648 This will allow you to load the configuration to the CP again. And after downloading and restart of CPU it should stay in RUN. But do not power off/on the CPU.Once the CPU is power off -> again the problem will rise... BR hristo |
7/28/2020 3:51 AM | |
Joined: 4/28/2015 Last visit: 3/21/2025 Posts: 16 Rating:
|
Hello, the CP343-1 lean version is very important. Plz check the module version with your soft HW configuration |
Follow us on