3/16/2017 2:59 PM | |
Joined: 10/18/2006 Last visit: 11/29/2023 Posts: 116 Rating:
|
Although the post is a bit outdated, the black plane connection between the CPU and the CP is the bottle neck. It is just 187,5 kBit/s! So it doesn't matter if you use an external CP343-1 or the MPI interface, the performance is the same. The only way to have better performance with S7-300 CPU is using the internal Ethernet / PROFINET interface on the CPU. If doing so, expect update cycle less 10ms. |
iba AG - Data Acquisition and Analysis the way it should be |
|
Follow us on