2/3/2006 2:57 PM | |
Joined: 4/3/2007 Last visit: 12/20/2024 Posts: 35 Rating: (5) |
Hi The CP343-1 LEAN supports S7 connections only in server functionality. That means you could make a put/get access from a plc (cp) which supports s7 connections. You could exchange your data over an iso-on-tcp connection by using FC5 "AG_SEND" and FC6 "AG_RECV" Please have a look at the following faq: http://support.automation.siemens.com/WW/view/en/16767769 kind regards |
Follow us on