6/3/2014 7:59 AM | |
Posts: 8946 Rating:
|
Yes, you can. |
6/4/2014 1:16 AM | |
Posts: 32 Rating:
|
The HMI is connected on the MPI bus.Is there any trick/config you have to do for reaching the HMI via the Lean card ? RGDS! |
6/4/2014 8:38 AM | |
Joined: 4/19/2008 Last visit: 11/21/2024 Posts: 1525 Rating:
|
Hello www.opauto.no, Have a Look on the FAQ, if you have one of the Shown Configuration it will work, How do you use WinCC flexible to transfer a project to an operator panel via S7 routing? More information on the topic of "Project transfer via S7 Routing" is available in the WinCC flexible manual in Entry ID: 18796010. |
Ammy |
|
This contribution was helpful to
1 thankful Users |
8/25/2014 4:02 PM | |
Joined: 4/29/2010 Last visit: 1/20/2025 Posts: 1557 Rating:
|
Hello, wich panel do you allready use and what do you exactly want to do (transfer,...)? With best regards |
8/27/2014 1:08 PM | |
Joined: 3/20/2013 Last visit: 3/18/2025 Posts: 676 Rating:
|
you have to add a PG/PC station in your project to get access to the HMI. add it, connect it to the CP, connect your physical ethernet adapter, download in the CPU, download to the HMI. edit: perhaps the link helps: http://support.automation.siemens.com/WW/view/en/45147695 |
Last edited by: Fafner at: 8/27/2014 1:10 PMBest Regards, |
|
8/29/2014 12:39 AM | |
Posts: 32 Rating:
|
Still no progress accorduing to the Procedure. I had an extra read thru. So i need simatic net to get the communication via CPU ? Rgds ØP
|
Follow us on