1/8/2007 10:17 AM | |
Joined: 5/21/2006 Last visit: 12/20/2023 Posts: 7 Rating: (0) |
Hello! I think the same, but don't have additional C-PLUG for test... Thanks. With best regards, Nechaev Alexey. |
1/12/2007 11:50 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (316)
|
Hi Nec, That is not fine, I believe there is also a update for the CP 443-1 Advanced. Yes, I have find it, Firmware Update V2.5 for CP443-1 Advanced you may do it by your self, disconnect the CP from the network and follow the description in the handbook very well. The firmware itself Firmware Update V2.5 for CP 443-1 Advanced (6GK7443-1EX40-0XE0). The handbook CP 443-1 Advanced for Industrial Ethernet / Manual Part B4Awith somewhere at the end the firmware update description. Hi, I forgot to say that it may help to load the firmware new, have you looked into the diagnostics of the CP? |
Last edited by: Late at: 1/12/2007 11:51 PMSomething forgotten.... I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|