6/16/2011 6:50 AM | |
Posts: 21 Rating:
|
Dear Experts, I am working on a PLC upgrading project. After study i select 6ES7 416-3XR05-0AB0 CPU with communication processor 6GK7443-1EX20-0XE0. Unfortunately CP card 6GK7443-1EX20-0XE0 is out of market and local supplier suggested 6GK7443-1EX11-0XE0 communication processor card. After study of 6GK7443-1EX11-0XE0 manual i am totally confuse because 416-3XR05-0AB0 CPU is not existing in his catalog. My Question is that the CP 6GK7443-1EX11-0XE0 will supported to 416-3XR05-0AB0 CPU. Please help me. Regrads, Automation Engineer AttachmentCP 443-1.pdf (61 Downloads) |
6/16/2011 7:08 AM | ||||
Joined: 4/19/2008 Last visit: 11/21/2024 Posts: 1525 Rating:
|
Hi Automation Engineer,
CP 443-1 Firmware Update V2.7 and Unrestricted Use on Every Hardware Release (6GK7443-1EX10-0XE0 and 6GK7443-1EX11-0XE0) May be you will find the more detail in the following Document/Link |
|||
Ammy |
||||
6/16/2011 7:19 AM | |
Joined: 10/7/2005 Last visit: 4/29/2025 Posts: 3047 Rating:
|
Hello Automation Engineer the 416-3XR05 CPU possible does not appear in the 443-1EX11 manual because it was relased some 6 years after the 1EX11 was released. It will most likely work asUMENCHOsuggested, but the question is: Why would you buy a CP that is out of production for almost two years (see HERE) fora new project (I hope your your supplier will sell it for a reallygood price)? You may also find the following useful as it will allow you find out what you are missing out on if you go for the ancient 1EX11 (e.g. it can NOT be used as a Profinet I/O Controller whereas the 1EX20 can). What differences are there between the Industrial Ethernet CPs of SIMATIC S7-400? I hope this helps |
Cheers |
|
Follow us on