5/8/2012 10:20 AM | |
Joined: 4/19/2008 Last visit: 11/21/2024 Posts: 1525 Rating:
|
Hello Plku, 6GK7443-1EX20-0XE0 is the new Released, Have a look here for more detail Differences. What differences are there between the Industrial Ethernet CPs of SIMATIC S7-400? Also What should you watch out for when changing from previous modules to the successor module CP443-1 (6GK7 443-1EX20-0XE0) or CP443-1 Advanced (6GK7 443-1GX20-0XE0)? |
Last edited by: Ammy at: 5/8/2012 10:22 AMLink For Migration Ammy |
|
5/8/2012 10:22 AM | |
Posts: 241 Rating:
|
Dear PLku as per/tf/WW/en/Posts/55077 Follow the link: if you are not using Full functions ofCP 443-1 (EX20)then you will not have any trouble replacing that with EX11. Also see https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&objId=26685738&objAction=csOpen&nodeid0=10904077&lang=en&siteid=cseus&aktprim=0&extranet=standard&viewreg=WWwhere you will find EX20 new functions. here is another but German.but you will find useful |
5/8/2012 12:56 PM | |
Posts: 947 Rating:
|
The most important difference - of EX20 - 15pin connector is delete. Also ex20 has a built in switch x2RJ45 and supports profinet |
7/12/2013 8:18 AM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating:
|
Follow-up-question splitted to wiring diagram from 15 pin to RJ-45 Best regards O_Moderator |
Follow us on