11/16/2009 3:50 PM | |
Posts: 35 Rating:
|
Im working on a project that uses two CP 443-5 Ext cards. Unfortunately when I open the PLC program in Simatic Manger I get error messages that the required version of this card is not in my hardware catalog. I have done a hardware update in Hardware Configuration by downloading all available updates and installing them. Still the CP 443-5 ext V6.4 card does not appear in the catalog. If any one can provide me with an update file for this card I would greatly appreciate it. Im also including some screen shots of the error messages and my hardware catalog. AttachmentCP 443-5 ext.zip (68 Downloads) |
11/17/2009 12:08 PM | |
Posts: 5822 Rating:
|
Hello, I fear you have to upgrade your STEP7 to V 5.4.5 to get it to work. You may find the Upgrade at: Service Pack 5 for STEP 7 V5.4 and STEP 7 Professional Edition 2006 I hope this will help you. Best regards J_Bell |
Follow us on