3/4/2017 6:41 PM | |
Joined: 9/27/2006 Last visit: 3/20/2025 Posts: 12344 Rating:
|
Hello José; What operating system are you trying to install your CP 5512 under? Hope this helps, Daniel Chartier |
3/5/2017 2:36 PM | |
Joined: 9/27/2006 Last visit: 3/20/2025 Posts: 12344 Rating:
|
Hello José; The CP 5512 should be compatible with Windows XP SP3 (32-bits). See the table in the following FAQ: Which SIMATIC NET PROFIBUS PC CP is compatible with which Microsoft Windows operating system? However, the interface for the CP 5512 is a Cardbus adapter (32-bits), whereas the adapter for the CP 5511 is PCMCIA (16-bit), so they are not compatible. And if your present laptop does not support Cardbus interfaces, you will not be able to use the CP 5512. The CP 5512 is discontinued since 2015, you will have very little support for it; the replacement is the CP 5711, USB-based. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 3/5/2017 2:37:08 PM |
|
Follow us on