9/4/2017 9:46 AM | |
Joined: 6/19/2008 Last visit: 8/6/2024 Posts: 46 Rating:
|
Hi Guys ! I don't want to start another topic so maybe I will ask here again - there is another problem. After installation of SP2 for PCS7 V7.0 now Windows and Station Manager (also PG/PS) can recognize this CP1623 card. The problem is that in Hardware Catalog I still can't find this CP card (see attached screens). So I can manually insert card into Station Configurator but not from hardware configuration... I've updated already hardware from here: But still I can's see CP1623 in hardware Catalog. Any ideas why ?? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 9/4/2017 5:43:53 PMNew subject after splitting |
|
Follow us on