6/4/2011 12:35 PM | |
Joined: 7/2/2008 Last visit: 2/26/2025 Posts: 928 Rating:
|
HelLo MavEric, As stated by Amit_86, you have to go for 6GK7443-1EX20-0XE0. You can use it as a direct replacement for your H-System without hardware modification. To read more check the following.
Best regards. H-H |
6/4/2011 6:48 PM | |
Posts: 947 Rating:
|
small addition: 6GK7443-1EX20-0XE0 has only RJ45-connectors and no have DSUB-15 connector |
6/4/2011 6:57 PM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating:
|
Well Gre_m Thanks for your suggestion but one has to go for it 6GK7443-1EX20-0XE0 if the Existing CP has failed. |
VANDE MATARAM..... |
|
6/7/2011 3:40 AM | |
Posts: 212 Rating:
|
hi Amit_86, there is difference in "Product cancellation" and "product discontinutaion". 1Ex11, is under LC phase of product cancellation. In such cases user is required to get in touch with Local SiemensOffice, for availability of modules. as its prodiuct cancellation many of the modules still must be available. and point to be noted, even after the product discontinuation techicnal support for the same for predefined time is available |
6/7/2011 10:18 AM |
|
Posts: 947 Rating:
|
Hi MavEric I agree ABN
Indeed the product removed from the sales, but it is available to replace 10 years. should contact to support |
Follow us on