6/19/2018 2:12 PM | |
Joined: 12/16/2015 Last visit: 5/31/2024 Posts: 7 Rating:
|
Hello Everyone, I am trying to connect with a mobile network (KPN) and a MQTT Broker and then send a message. I am using:
I have succeed in doing this, but the only problem is the stability. Sometimes I can connect straight away with the Mobile network and the Broker, but sometimes it takes very long or I get a timeout. I dont know what s causing the problem. Things that I have checked:
If i setup the connection through TCP/IP from the PLC (so without the card and straight to wired internet) with the same settings the connection is effortless and works straight away. I am not getting any errors from the online diagnostics from the card. Attachmentscreenshots.zip (100 Downloads) |
8/11/2020 3:44 PM | |
Joined: 8/3/2009 Last visit: 3/19/2025 Posts: 15032 Rating:
|
Hello perhaps you will find help in the Basic FAQ to this Topic: https://support.industry.siemens.com/cs/de/en/view/109772284 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on