9/8/2008 12:16 PM | |
Joined: 3/21/2006 Last visit: 3/2/2023 Posts: 10221 Rating:
|
Hi About PC side maybe this FAQ will help you: How do you set up a Fetch/Write connection (S5-compatible communication) to the SIMATIC S5 via Ethernet for the SIMATIC NET OPC server About S5 side: Yes you must new number job in CP143 COMM linked with new address of PC station. After that, in S5 program you must define new FETCH and RECEIVE blocks which correspond to number's job, of course maybe with defferent data area (other Data Block). More details in part 6: CP 143 TF with NCM COM 143 TF Volume 1 of 2 regards |
9/11/2008 8:48 PM | |
Posts: 5822 Rating:
|
Dear Apel, are you sure about the remote SSNR? Is it possible you talk about TSAP? Because now I am confused. Best regards J_Bell |
9/12/2008 3:46 AM | |
Posts: 241 Rating:
|
Dear Mr.J_BELL, I confussed you,Great! In case of Fetch I used TSAP: READREAD and for RECEIVE i used WRITWRIT.For both case the remote address:0000000.Please look into the following picture(Print-Screen)-attached. AttachmentMY NEW ADDED JOB RCV-SEE REMOTE.zip (62 Downloads) |
Follow us on