1/8/2008 7:24 AM | |
Joined: 5/25/2007 Last visit: 12/11/2024 Posts: 83 Rating: (3) |
Hello: Buzz LightYear |
1/8/2008 9:21 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (319)
|
Hi, A maximum of 64 connections could be made with the CP1613(A2). See the handbook SIMATIC NET Produktinformation Industrial Ethernet S7-1613/Windows V6.0 for more information. See on page 66 the information...
A maximum of 4 CP 1613 modules can be operated in a PG/PC at any one time.
The number of applications that can be run at the same time depends on the interface used. |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
1/9/2008 1:56 AM | |
Joined: 5/25/2007 Last visit: 12/11/2024 Posts: 83 Rating: (3) |
Dear Late: Best regards Buzz LightYear |
Follow us on