10/14/2008 3:03 PM | |
Posts: 12 Rating: (0) |
Hi all My two CP1616s do not work soon after PC rebooted during commssioning. HW config is for iba PDA of Sinamics CU320 with CBE 20s. I can't ping them. I tried toattatched experts advice. but not work. /tf/WW/en/Posts/10304 Any body have the tool for completely reset CP1616? I cant find out the dev. Kit metioned in attached thread. Do i have to buy new CP1616 instead of fixing? Help. |
10/15/2008 12:08 AM | |
Posts: 5822 Rating: (412)
|
Hello, do you have the Dev. Kit available at this Update: Software Version V2.1 for CP 1616 and CP 1604 incl. Windows Driver Released for Delivery or which version of the Dev. Kit do you use with the CP? Best regards J_Bell |
10/15/2008 6:09 AM | |
Posts: 12 Rating: (0) |
Thanks for your reply. I do not use dev.kit. My application iba PDA use CP1616 as it's IO Driver. Is there any other way instead using dev.kit? |
Follow us on