Industry Online Support
Technical Forum
4/30/2010 11:16 AM | |
Joined: 4/5/2006 Last visit: 3/18/2023 Posts: 917 Rating:
|
Hi Kargan, here few links to check compatibility of CP1623 with OS and SIMANTIC NET: Which SIMATIC NET Industrial Ethernet PC CP is compatible with which Microsoft Windows operating system? Restricted Delivery Release for the SIMATIC NET PC CP1623 Module This document says: "The only precondition is the use of the SIMATIC NET CD with version 2007 + Hotfix 1 or higher." regards |
8/30/2011 7:58 AM | |
Joined: 3/21/2006 Last visit: 3/2/2023 Posts: 10221 Rating:
|
Hello, Yes, you are right. SN7.0 HF1 is compatible with PCS7 7.1. More at PCS 7 V7.x Kompatibilitätsliste. Best regards, Hristo Mihalev |
8/31/2011 3:40 PM | |
Joined: 4/8/2009 Last visit: 11/11/2022 Posts: 9 Rating:
|
Thanks for your answer UMENCHO. |
Follow us on