6/25/2010 9:06 AM | |
Joined: 4/24/2006 Last visit: 3/21/2025 Posts: 8904 Rating:
|
Dear Solutio Riders, When you have used CP340 and Modbus, someone has written the driver. Siemens offer a loadable driver Modbus RTU for CP341: MODBUS Software license for CP 341/ CP441-2 Here are two manuals: SIMATIC S7-300/S7-400 Loadable Driver for Point-to-Point CPs: Modbus protocol, RTU format, S7 is Slave SIMATIC S7-300/S7-400 Loadable Driver for Point-to-Point CPs: Modbus protocol, RTU format, S7 is Master Best regards, Wizard |
Last edited by: Wizard at: 6/25/2010 9:09 AM |
|
6/25/2010 10:45 AM | |
Posts: 3093 Rating:
|
Hello Sulution Riders, the loadable drivers for Modbus RTU can be used with CP341 and have to be ordered separately. Regards, Kaulquappe |
6/25/2010 1:05 PM | |
Joined: 9/27/2006 Last visit: 3/22/2025 Posts: 12344 Rating:
|
Sorry, R J; The information you have provided only applies to a CP 341 (or a CP 441-2 in a S7-400 system). It cannot be used on a CP 340. No Siemens "Loadable drivers" can besetup in the CP 340. http://support.automation.siemens.com/WW/view/en/1918186 If you want to use a CP 340 with Modbus, you must provide the functions that willimplement the driver. Hope this helps, Daniel Chartier |
6/28/2010 12:41 PM | |
Joined: 1/17/2007 Last visit: 3/10/2025 Posts: 1557 Rating:
|
There is indeed a free ASCII protocol available for the CP340. You need to download the PtP parameterisation software to use it. However, any protocol requirements (e.g. mobus) would have to be realised with a driver developed in AS block(s) that you code yourself. I have developed a modbus driver that works with the CP340 (and also 341 and 441 and PtP CPU's), so it can be done. Although mine took about a year to develop (but it does act as master or slave and also works over TCP). I suppose a slave driver that works only with the CP340 could be developed by a capable programmer in I would estimate 3-4 months. |
Programming today is the race between software engineers building bigger and better idiot proof programs, and the universe producing bigger and better idiots. |
|
This contribution was helpful to
1 thankful Users |
Follow us on