Industry Online Support
Technical Forum
3/10/2009 6:36 AM | |
Posts: 557 Rating: (64) |
hi you can check following posibility: 1) CPU scan time. 2) cp340 output spikeprgram you can put is OB 35 & Change the time in two posibility: a) in hardware configuration change scan time 50ms b) in hardware configuration change scan time 5ms if your plc scan is suppose 50 ms that mean in 1 sec 20 scan per sec if it is 5ms that mean in 1 sec 200scan ,so check these posibility & tell me the result, & also send me the diagnostic buffer. regards vivek |
Follow us on