7/6/2012 4:15 PM | |
Posts: 11 Rating:
|
Dear Experts, I'm working on module CP340 and I want to configure parameter. I downloaded PtP V5.1 sp12 from this link(https://support.automation.siemens.com/WW/llisapi.dll/57026339?func=ll&objId=57026339&objAction=csView&nodeid0=37217116&lang=en&siteid=cseus&aktprim=0&extranet=standard&viewreg=WW&load=content) and installed in my pc after click to run parameter configure, Step7 show the messege s7fptp.sdb not found as file I attached , I installed to my two pc one works fine but another got this messege, please help. Thank you Preeja
|
7/6/2012 4:54 PM | |
Joined: 1/28/2009 Last visit: 3/8/2025 Posts: 6860 Rating:
|
Hello , Did you check these requirements?
Best regards Hamid Hosseini |
7/6/2012 5:25 PM | |
Posts: 11 Rating:
|
Hellohdhosseini, Oh, so sorry I pasted wrong link. Actually, what I mean is this link https://support.automation.siemens.com/WW/llisapi.dll/27013524?func=ll&objId=27013524&objAction=csView&nodeid0=24255094&lang=en&siteid=cseus&aktprim=0&extranet=standard&viewreg=WW&load=content I downloaded to configure CP340 on my project, my two PC installed "PtP Param V5.1 incl. SP12" one works fine, I mean can configure CP340 parameter, but another one got the messege as attachment below. Software I've got in two pc are the same "Step7 BASIS v5.5, and Step7 Pro 2010 v5.5", the missing file in the messege I can search and find it also. Best Regard, Preeja
|
3/9/2017 8:52 AM | |
Posts: 2 Rating:
|
Simply Run Simatic manager as administrator. ;) |
This contribution was helpful to
1 thankful Users |
Follow us on