6/26/2007 12:07 AM | |
Joined: 1/7/2006 Last visit: 12/23/2024 Posts: 2705 Rating:
|
Dear Grant, 1) Is it possible to communicate to more than one device using the Siemens 3964R protocol with RS422. If so how do you configure the blocks FB7 (P_RCV_RK) and FB8 (P_RCV_RK) to know which device to communicate with. From my studying on the forums and product documentation I am leaning towards this being a Modbus Master aswell even though the existing drawings suggest otherwise. Answer 1) I think that that is not possible, this because there is no address forseen in the protocol, so thats not possible. Was that before on the S5 possible???? 2) How do you set up the Modbusslave configuration in Netpro to communicate to the Modbus Master (CP341). I have tried to add a other device in step 7 with PTP interface but I can only add 2 devices on the PTP network. I understand that it is point to point but there is no Modbus interface to choose from. Answer 2) Normally on a RS485 bussystem you can program more slaves, they call it a Multidrop bus. Please look also to my answers on the Modbus Network in this Forum. |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on