10/5/2008 4:15 PM | |
Posts: 15 Rating: (2) |
Dear Experts, I have two CPUs S7-400 (redundant) and five CP341 (two works as Modbus Master and three works as Modbus Slave). I am using Step7 V5.3 + SP3. I upgraded the software: Simatic S7 CP PtP Param to 5.1 SP8 Simatic S7 CP PtP Modbus Master to 3.1 SP4 Simatic S7 CP PtP Modbus Slave to 3.1 SP5. FB7 P_RCV_RK is version 3.0 and it has 3142 work memory, and Last Interface Change date is 14.08.2007. FB8 P_SND_RK is version 3.0 and it has 2876 work memory, and Last Interface Change date is 14.08.2007. After the upgrade and I saved the new FC 7 y FC 8 in CPU,I have two errors in CPU: Area length error when reading Area length error when writeing You can see these errors in attach file. What should I do to clear the errors? AttachmentError.zip (306 Downloads) |
Last edited by: Banxico at: 10/5/2008 4:17 PM |
|
10/5/2008 9:03 PM | |
Posts: 15 Rating: (2) |
Hi edr, |
10/16/2008 10:41 AM | |
Posts: 5822 Rating: (412)
|
Hello, did you already check this Download? Download CD "CP340, CP341, CP440, CP441" The SP 9 is already available. I did not completely notice that you have not the latest version. Best regards J_Bell |
Last edited by: J_Bell at: 10/16/2008 10:43 AM |
|
Follow us on