7/12/2009 2:49 AM | |
Joined: 1/17/2006 Last visit: 1/14/2025 Posts: 554 Rating: (29) |
Hello, I have to send/receive data (15 bytes)between CP341 and one DataMatrix reader via ASCII driver. I downloaded the manual on the following link: http://support.automation.siemens.com/WW/view/en/1117397 In this manual there are explanations using the following blocks that I could not find on the STEP7 Libraries. Where can I find them ? Or, what is the best way (which blocks) to exchange ASCII serial data using CP341 (6ES7341-1AH02-0AE0)? Maybe any project example !! - FC 5 V24_STAT - FC 6 V24_SET
- FB 8 P_SND_RK
|
"Educate the children and it won't be necessary to punish the men." |
|
7/12/2009 5:40 AM | |
Posts: 261 Rating: (42) |
Hi, You need to install the PTP communication driver CD. Then you will find
We can use all these System Function Blocks with the ASCII Driver: FB P_SND_RK FB P_RCV_RK FC V24_STAT FC V24_SET Regards ddg AttachmentCP341.pdf (375 Downloads) |
7/12/2009 7:02 PM | |
Posts: 261 Rating: (42) |
You can find the CP PTP S/W in this link. Sorry, I have no idea about other blocks. Regards ddg |
Last edited by: ddg at: 7/12/2009 8:01 PM |
|
Follow us on