Industry Online Support
Technical Forum
10/2/2009 10:58 AM | |
Posts: 2 Rating: (0) |
HI we have CP341(6ES7 341-1CH01-0AE0) in my site and i write FB (used FB8 & FB7) and DB for CP341 then download to cpu . i see the TXD led are blinking and RXD is off (there are not any connection between CP341 and slave).then i modify FB and delete old DB and create new DB then download to cpu but i see TXD is off and in FB all is ok and output of ERROR in FB8 is zero but in Module information -CP341-RS422/485 error IF1:Receive Error Event ID:16#F1C8:0830 . what i do to slove this problem and clear this error. thanks Attachmentcp341.zip (161 Downloads) |
Follow us on