3/8/2018 6:39 AM | |||
Joined: 1/2/2014 Last visit: 3/27/2025 Posts: 149 Rating:
|
ThanksKaulquappe for the detailed reply. I have one more question. While opening the old backup and clicking on the parameter a message is showing as in the picture attached. "The version of the driver saved in proj SDB is different than the version of the driver installed on the programming device". cp341 is old version 6ES7341-1CH01-0AE0 Currently, I have installed the latest version in my PC from this link
I believe no need to re-download driver to CP card since its already done in the old configuration and keeping the old IO address 256. Please correct me if I am wrong. What are the procedures to be followed if Driver re-download is needed? Can I use the newest parametrization software V5.1 + SP14 for the old CP341 with same logic program and parameters ? |
||
Last edited by: RIAN Che at: 3/8/2018 7:01:22 AM |
|||
Follow us on