3/17/2014 2:56 PM | |
Joined: 3/20/2013 Last visit: 4/16/2025 Posts: 676 Rating:
|
Hey, 1. you do not need the advanced CP for simple TCP/IP connections you can also use the simple one. 6GK7343-1CX10-0XE0
Note: With the AG_Send and AG_Recv blocks it is very difficult to implement different length of telegrams. The easiest way is to go with a CPU that can speak via Ethernet and to use the TCON, TSEND/TUSEND, TDISCON blocks 2. that is a good question, afaik there is the possibility to simulate communication. But i did not try it yet, so perhaps somone else can help you. 3. --> 2. ... sry ;) |
Best Regards, |
|
3/17/2014 5:14 PM | |
Posts: 3093 Rating:
|
Hallo Tomy Master, it is not possible to simulate communication with PLCSIM. Regards, Kaulquappe |
Follow us on