1/31/2019 6:04 PM | |
Joined: 3/12/2014 Last visit: 3/6/2025 Posts: 21 Rating:
|
Hello. For the past week I have been trying to configure I-Device communication between a CP343-1 and a CP343-1 Lean. I have been able to get the configuration to work single sided (the lean will transmit up, but the 343-1 will not transmit to the lean). I am using PNIO-Send and PNIO-Recieve on both CPU's. To test my configuration I first removed the 343-1 from the configuration and connected the lean module by I-device directly to the CPU (using the CPU as I-Device Controller). All worked well. I reversed the configuration, using the CP343-1 as the I-Device controller, and setup the CPU as the I-Device and I have the same issue as when trying to communicate between the two CP's (The 343-1 will not transmit data to the CPU, only receive). I upgraded the firmware of the CP 343-1 to the most recent version, and the issue remains. I have been reading the help files and manuals and am at a loss; attached is my project; any help appreciated. AttachmentTest4.zip (105 Downloads) |
1/31/2019 6:06 PM | |
Joined: 3/12/2014 Last visit: 3/6/2025 Posts: 21 Rating:
|
A screenshot of the web diagnostic screen on the 343-1 as controller. |
Follow us on