4/20/2010 10:06 PM | |
Joined: 9/19/2009 Last visit: 12/23/2024 Posts: 459 Rating: (85) |
Hello yanikita I have Step7 V5.4 sp4 and I don´t have any problem. I have this CP. Regards. JM |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
4/21/2010 1:55 AM | |
Joined: 10/7/2005 Last visit: 1/13/2025 Posts: 3029 Rating: (1058)
|
Hello yanikita Below is an excerpt straight from THIS release note which explains your problem: To be able to use the full scope of functions of the CP 343-1 (order no. 6GK7343-1EX30-0XE0) you require STEP 7 V5.4 SP1 + HF2 plus Hardware Support Package (HSP), or a later version of STEP 7. I hope this helps. |
Cheers |
|
This contribution was helpful to1 thankful Users |
4/21/2010 8:21 AM | |
Posts: 19 Rating: (0) |
Hi everybody, Thanx for your help. I will have to change this CP for the 1EX21 one... I will have to wait to use Step7 V5.4 Regards. Yanikita |
Follow us on