9/30/2008 6:12 PM | |
Joined: 5/7/2008 Last visit: 1/3/2025 Posts: 30 Rating: (1) |
Hi, I am trying to comunation data transfer between two S7-300s, using ethernet connection ,tcp connection . I dont know what Im doing wrong. Could somebody help me how to estabilish communication as simple as is possible? My hardware: CPU 315C-2 DP (315-2AG10-0AB0) on both PLCs CP 343-1 Lean (343-1CX10-0XE0) model the same but different firmware version: V1.0 on PLC1 and V2.6on PLC2 By this time I have connected both PLCs with cross-connection cable,then configured in NetPro the ISOonTCP connection and I also used FC5 and FC6 function blocks. I put FC5 on OB1 in first PLC and FC6 in second one and nothing. The sending function was giving back alternatingly the status word of 8183 and 8180. where is the problem my project send you looking Thanks. AttachmentHaberl_1.zip (316 Downloads) |
Last edited by: seceem at: 9/30/2008 6:19 PMLast edited by: seceem at: 9/30/2008 6:17 PMLast edited by: seceem at: 9/30/2008 6:13 PM |
|
9/30/2008 7:04 PM | |
Joined: 7/15/2008 Last visit: 12/12/2024 Posts: 382 Rating: (44) |
Hello ,
c.) you have no connection between the two CP Cards. |
Last edited by: legacy support at: 9/30/2008 7:29 PM |
|
9/30/2008 10:23 PM | |
Posts: 196 Rating: (12) |
Hi Sorry i was to fast, but i still recomend to use two connection. |
10/19/2008 10:32 PM | |
Posts: 5822 Rating: (412)
|
Hello Seceem, would you mind telling if the download of the Connectiontable was solving your issue. You had to download it twice. Best regards J_Bell |
Follow us on