3/26/2008 9:26 AM | |
Joined: 4/10/2006 Last visit: 1/22/2025 Posts: 947 Rating: (2) |
Hallo!!
I connected for the first time a CP343-1 Leane (code 6GK7 343-1CX10-0XE0) with a PC Gefran Digistar II, via ethernet. I attached the configuration. Is it correct? If it is correct, how I write / read from bits of PC plc? What do I need to read and write bits in plc, using the PC Gefran II? In this system i use a cpu 313C. Thanks for help.... Attachmentconfigure.pdf (418 Downloads) |
Setting of my PG M6 Siemens |
|
3/26/2008 11:03 AM | |
Posts: 5822 Rating: (412)
|
Dear Roby, here you can use Industrial Ethernet and it works just like with SOFTNET S7 for PROFIBUS just other Addresses and a Standard NIC instead of the CP 5X11. Best regards J_Bell |
3/26/2008 11:07 AM | |
Joined: 4/10/2006 Last visit: 1/22/2025 Posts: 947 Rating: (2) |
But I have the impression that it will be difficult to set the cp343 with sofnet ... I had already struggled with the very cp5611 ... There is a manual that talks about this? Hallo.... |
Setting of my PG M6 Siemens |
|
3/26/2008 11:20 AM | |
Posts: 5822 Rating: (412)
|
Dear Roby, try this FAQ: How do you configure an S7 connection for a user application via Industrial Ethernet with the SIMATIC NET PC software? Best regards J_Bell |
3/26/2008 11:34 AM | |
Joined: 4/10/2006 Last visit: 1/22/2025 Posts: 947 Rating: (2) |
Thank J_Bell... Roby |
Setting of my PG M6 Siemens |
|
3/27/2008 9:03 AM | |
Joined: 4/10/2006 Last visit: 1/22/2025 Posts: 947 Rating: (2) |
Hello J_Bell ... I followed the explanation of the FAQ:
|
Setting of my PG M6 Siemens |
|
3/27/2008 10:18 AM | |
Posts: 5822 Rating: (412)
|
Dear Roby, I guess one of the following is not checked with your configuration.
Best regards J_Bell |
3/27/2008 10:47 AM | |
Joined: 4/10/2006 Last visit: 1/22/2025 Posts: 947 Rating: (2) |
OK....... For the moment, everything's OK....
Hallo, J_Bell! Very thanks... Roby |
Setting of my PG M6 Siemens |
|
Follow us on