Industry Online Support
Technical Forum
12/27/2009 10:40 AM | |
Posts: 7 Rating:
|
Dear All, Does S7 400-H supports CP441-1 as Modbus RTU Slave? If Yes Apart from Modbus slave driver what is required to be done? Please Help! Regards, Eqbal |
1/4/2010 1:54 AM | |||||
Joined: 8/1/2008 Last visit: 10/24/2023 Posts: 40 Rating:
|
Hi eqbal Sorry for late answer. Your Question Do you support the CP441-2 is redundant? Answers. It is Support. Note: MODBUS Driver CP441-2 is when you download. Need to download each one. For more information, MODBus Please refer to the documentation. modbus master (RTU)
modbus slave (RTU)
I hope you could help us |
||||
Follow us on