9/14/2007 12:31 PM | |
Posts: 14 Rating:
|
Also, I am now confused as to which Firmware version it is running. When I open the Properties ON-LINE, it shows me Version 2.6 - see attachment |
9/14/2007 12:42 PM | |
Posts: 5822 Rating:
|
Hello, yes, you still run the old version of the CP even so you configured the latest one. STEP 7 should have shown you a warning saying that you configure the wrong version of the CP, didn't it? To upgrade the CP to the latest version, please use this FAQ: CP 443 -1 Firmware Update V2.6 and Unrestricted Use in any Hardware Release (6GK7443-1EX10-0XE0 and 6GK7443-1EX11-0XE0) The "how to" is explained in the FAQ. I would really recommend the update of the CP to this version. Best regards J_Bell |
Follow us on